This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sorry about the delay.
Symbol ramp time: For OOK extra "symbol(s)" are added before the start of the packet to ramp from off state to the programmed output power. "Symbol ramp time" is the length of the extra "symbol" added.
ASK/ OOK shape length: This is the portion of a symbol used to ramp up to a logic '1'. Example: If this is set to 1/4, 1/4 of the symbol length is used to ramp up, then 3/4 of the time sending max power and then 1/4 of the time ramping down.