This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please help: CC1110 simpliciTI AP-as-Hub code

Other Parts Discussed in Thread: SIMPLICITI

I have problem with add new interrupt in Ap-as-Hub code of SimpliciTI like this

#include "bsp.h"
#include "mrfi.h"
#include "nwk_types.h"
#include "nwk_api.h"
#include "bsp_leds.h"
#include "bsp_buttons.h"
#include "nwk_pll.h"
#include <hal_cc8051.h>
#include <ioCCxx10_bitdef.h>
#include <ioCC1110.h>
#ifndef APP_AUTO_ACK
#error ERROR: Must define the macro APP_AUTO_ACK for this application.
#endif

void toggleLED(uint8_t);

static void linkTo(void);

//static uint8_t sTid = 0;
static linkID_t sLinkID1 = 0;

#define SPIN_ABOUT_A_SECOND NWK_DELAY(1000)
#define SPIN_ABOUT_A_QUARTER_SECOND NWK_DELAY(250)
#define PIN BIT5
/* How many times to try a Tx and miss an acknowledge before doing a scan */
#define MISSES_IN_A_ROW 2

#pragma vector = P1INT_VECTOR
__interrupt void p1_ISR(void)
{
// Note that the order in which the following flags are cleared is important.
// For level triggered interrupts (port interrupts) one has to clear the module
// interrupt flag prior to clearing the CPU interrupt flags.

P1IFG &= ~PIN; // Clear status flag for pin
P1IF = 0; // Clear CPU interrupt status flag for P1

P1_0 ^= 1; // Toggle SRF04EB LED3

}

After building, I got  Error[Pa045]: function "p1_ISR" has no prototype 

Please help me