Other Parts Discussed in Thread: CC1101, CC1190
Are there any figures about the bias current on a CC1190? I've built some prototypes following the CC1101+CC1190-868MHz reference design but My CC430-based radio is not receiving anything. I have not the necessary RF equipment to measure the LNA_IN/OUT lines so I wonder if looking at the bias current would tell me if the CC1190 is working or not. FYI, I'm reading around 24uA with LNA = HGM = 1.
Another issue is that I was unable to source 4.1 nH inductors for L24 (last series inductor before the antenna) so I ended by mounting a 3.9 nH on my three boards. Could this be killing my signal? I'm more used to other RF frontends like the CC1101 and they tend to provide very flexible performances, at least during the prototyping stage. On the other hand I'm finding the CC1190 to be a very tricky IC.
Thanks in advance for your suggestions.