This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The interval of sending packet ...

Other Parts Discussed in Thread: CC1101

Smart RF Studio 7:

''  The packet interval option can be used to change the delay time between each packet. When the "Use default" is checked, the value calculated by SmartRF Studio is shown.... ''

My question : In what way is it possible to ensure that the time between packets is less than 150 msec. - As given in the Smart RF Studio 7  ?!! ... 

(If at all CC1101 can send packets faster than 150mseč - for example, to 25 msec)

If so - how to set registers CC1101 ...
(Write if you can and example programs ...)

Thanks in advance ...

Best regards ...

  • Hello Sasa,

    Just un-check the box and lower the interval. This parameter is related to the PC SW execution of SmartRFStudio. You do not need to change any registers as they are not related to this change. There is a limit to how fast studio can send packets, but 25 ms might work.