Hi,
So far I used cc2500em msp430f5529 evaluation board with the following settings : RF frequency 2400 MHz, MSK modulation, 250 kbps data rate, 540kHz rx filterbandwidth ( I attached the register setup code) when I used that setting everything worked fine, but when I started to use cc1101em with the following settings: RF frequency 868 MHz, MSK modulation, 250 kbps data rate, 540kHz rx filterbandwidth ( I attached the register setup code for it to) I succeed to receive several message from the sender and after several message the sender got stuck on the line code :
"while (!(TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN));" of the the attached RFSendPacket function and stop sending messages. I will be glad if someone may have any ideas what may cause it and what should I do for solving it.
Thanks
Roy
void RFSendPacket(char *txBuffer, char size)
{
TI_CC_SPIWriteBurstReg(TI_CCxxx0_TXFIFO, txBuffer, size); // Write TX data
TI_CC_SPIStrobe(TI_CCxxx0_STX); // Change state to TX, initiating
// data transfer
while (!(TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN));
// Wait GDO0 to go hi -> sync TX'ed
while (TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN);
// Wait GDO0 to clear -> end of pkt
TI_CC_GDO0_PxIFG &= ~TI_CC_GDO0_PIN; // After pkt TX, this flag is set.
// Has to be cleared before existing
}
my CC2500 register setting:
void writeRFSettings(void)
{
// Write register settings
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG2, 0x0B); // GDO2 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG0, 0x06); // GDO0 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTLEN, 0xFF); // Packet length.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL1, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL0, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_ADDR, 0x01); // Device address.
TI_CC_SPIWriteReg(TI_CCxxx0_CHANNR, 0x00); // Channel number.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL1, 0x07); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL0, 0x00); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ2, 0x5D); // Freq control word, high byte
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ1, 0x93); // Freq control word, mid byte.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ0, 0xB1); // Freq control word, low byte.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG4, 0x2D); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG3, 0x3B); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG2, 0x73); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG1, 0x22); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG0, 0xF8); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_DEVIATN, 0x00); // Modem dev (when FSK mod en)
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM1 , 0x3F); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM0 , 0x18); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_FOCCFG, 0x1D); // Freq Offset Compens. Config
TI_CC_SPIWriteReg(TI_CCxxx0_BSCFG, 0x1C); // Bit synchronization config.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL2, 0xC7); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL1, 0x00); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL0, 0xB2); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND1, 0xB6); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND0, 0x10); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL3, 0xEA); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL2, 0x0A); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL1, 0x00); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL0, 0x11); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSTEST, 0x59); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST2, 0x88); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST1, 0x31); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST0, 0x0B); // Various test settings.
}
// PATABLE (0 dBm output power)
extern char paTable[] = {0xFB};
extern char paTableLen = 1;
my CC1101 register setting:
void writeRFSettings(void)
{
// Write register settings
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG2, 0x0B); // GDO2 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_IOCFG0, 0x06); // GDO0 output pin config.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTLEN, 0xFF); // Packet length.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL1, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_PKTCTRL0, 0x05); // Packet automation control.
TI_CC_SPIWriteReg(TI_CCxxx0_ADDR, 0x01); // Device address.
TI_CC_SPIWriteReg(TI_CCxxx0_CHANNR, 0x00); // Channel number.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL1, 0x0C); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCTRL0, 0x00); // Freq synthesizer control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ2, 0x21); // Freq control word, high byte
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ1, 0x62); // Freq control word, mid byte.
TI_CC_SPIWriteReg(TI_CCxxx0_FREQ0, 0x76); // Freq control word, low byte.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG4, 0x2D); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG3, 0x3B); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG2, 0x73); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG1, 0x22); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_MDMCFG0, 0xF8); // Modem configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_DEVIATN, 0x60); // Modem dev (when FSK mod en)
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM1 , 0x3F); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_MCSM0 , 0x18); //MainRadio Cntrl State Machine
TI_CC_SPIWriteReg(TI_CCxxx0_FOCCFG, 0x1D); // Freq Offset Compens. Config
TI_CC_SPIWriteReg(TI_CCxxx0_BSCFG, 0x1C); // Bit synchronization config.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL2, 0xC7); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL1, 0x00); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_AGCCTRL0, 0xB0); // AGC control.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND1, 0xB6); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FREND0, 0x10); // Front end RX configuration.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL3, 0xEA); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL2, 0x2A); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL1, 0x00); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSCAL0, 0x1F); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_FSTEST, 0x59); // Frequency synthesizer cal.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST2, 0x88); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST1, 0x31); // Various test settings.
TI_CC_SPIWriteReg(TI_CCxxx0_TEST0, 0x09); // Various test settings.
}
// PATABLE (0 dBm output power)
extern char paTable[] = {0x50};
extern char paTableLen = 1;