Dear sir,
I'm testing the receive mode of CC1101(433MHz) with TrxEB.
My procedures are as follows:
1. Connect the CC1101 module from TI to TrxEB EK board and then connect USB cable to PC.
2. Turned the SmartRF studio7.
3. Checked the recognization of device(it's ok)
4. Select the "Generic 868MHz" and then change the frequency to 403MHz.
5. Select the "Continuous RX" and then change the data format to "Synchronous serial mode".
6. Set value of parameter of the signal generator as same as the values of RF parameters on SmartRF studio.
7. Finally, connected the probe of oscilloscope to GPIO0, GPIO2 on the TrxEB to check the signal.
** Here was my result
1. when the "Continuous RX" and then change the data format to "Synchronous serial mode".
2. The amplitude of signal generator was the -50dBm.
3. The RSSI on SmartRF studio was -38dBm.
4. But, GD2 is 1.2KHz and GD0 is 3.3V(Not changed)
On your CC1101 datasheet, GD2 is clock when IOCFG2 = 0x0B and GD0 is data when IOCFG0 = 0x0C
** Here was my question:
Why was GD2 measured with 1.2KHz and why was GD0 not changed?
Please, give your advice to me a.s.a.p.
B&R