This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windows CE driver for CC1111

Does anyone have a Windows CE driver for CC1111.  Windows CE does not have the usbser.sys driver and the example code is not very helpful.  The CC1111 being compatible with the CDC was brilliant but M$ got distracted with other issues and didn't provide support for it under Windows CE 6.0.  If one is not available could someone provide some guidance on where to start? Thanks