Hi
I'm making wireless intercom with CC1125.
The parameter is as below
Frequency : 430~480MHz
Modulation : MSK,4GFSK
DATA Rate : 70Kbps
Deviation : 17.5KHz
Channel Bandwidth : 156.25KHz
Front-end module : RFFM6403
MY device is working well under 470MHz.
CC1125 Datasheet say it guarantees 410~480MHz.
But the behavior is different in 470~480Mhz......lose signal easily, noisy.....etc...
I've checked RF part from CC1125 to RFFM6403. There is no problem. Antenna as well
Can you give me any advice about this problem?
Regards,
Cha