Hi,
are the series 10k resistors on the CC1190+CC1120 EM for the control signals; LNA_EN, HGM and PA_EN, necessary when connecting them directly to an MCU? I guess the reason why they are present on the EM is for ESD protection due to the human touchable pinrow or perhaps it is used as a current limiter if interfacing to 5V logic...?
Regards, HC