This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC LM35 on CC1111

Other Parts Discussed in Thread: LM35

Hi, 

i use the LM35 and the ADC from CC1111.

Do you think my misstake is, that i calculate wrong? For example, i configurate my ADC with 10 Bits. That is 2^10= 1024. My LM35 has a spectrum of 2degree to 150 degree. Also 148 degree. I think i have to divide it. Also 148/1024. Now i have one bit resolution. 

After that i have to multiply the ADC result with this one bit value. After that multiplay it with 100. İs that right?

But i don't anderstand. My LM35 gives me a value for example 300mV/C. And that is my degree. I have to multiplay it with 100 only. Then i have 30 degrees. But what did my ADC with the 300mV/C value? It makes it digital. That means i have not more 300mV/C, i have what?

If i make the calcuation which i wrote, then i won't get 30 degrees. What is wrong?

Please help