I am using CC430 as Tx and receiving with CC1101. The SmartRF Studio 38.4K@868Mhz suggestions works fine but we would need 4-5 dB more as link margin. We cannot modify TX, but we can operate on Rx side. I would prefer CC1101+CC1190 because the FW modification is minimal. Which is the best choice from the link budget point of view? Is there any AN on passing from CC1101 to CC1125? Do you have an evaluation board of CC1125 other than http://www.ti.com/tool/cc1125dk ? I would need only the CC1125 shield and not the whole kit.
Thanks
Mirko