Hi,
I am trying to use timer 1 or timer 3 in modulo mode to generate an interrupt. Even though the timer counts upto TCC0 an interrupt is not generated. The same code works fine on a CC2510 for timer 3. Since there are are no changes in timer 3 registers in CC2530 i expect the same code to work here too. But as i mentioned there is no interrupt generated. Kindly let me know whether you have faced this problem too and any suggestions to over come the same are welcome.
thanks..
kannan..