Hello,
I have four questions about the register access in eWOR mode on CC1121.
1. In the SLEEP state (by the SWOR strobe), what does eWOR behave when the MCU access to a register in CC1121?
Does eWOR mode stops because CSn is pulled to low?
2. When state is in SLEEP (with SWOR strobe) and the MCU access to a register (read or write), the automatic state transition (from SLEEP, through IDEL, to RX) stops.
Is this a valid behavior?
3. In RX mode, despite the MCU access to a register, the state remains in RX.
In the case of eWOR mode, does CC1121 not remain in the SLEEP state by a register access?
4. If the automatic state transition stops (the eWOR mode finishes) by a access from MCU, should I send a SWOR strobe to CC1121 to restart the automatic state transition?
Best Regards.
Nomoto