Hi,
I'm using the CC1120 transceiver with a TCXO for a low power application.
I would like the TCXO to be OFF when the cc1120 is in sleep mode and to wake up automatically with the CC1120.
The TCXO doesn't have an enable pin.
On the CC1120_CC1190_868_EM design a zero ohm resistor (R321 not mounted) can connect the TCXO's vcc to the DCPL_XOSC pin of the CC1120.
I've measured about 1.8V on the DCPL_XOSC when the CC1120 is not in sleep mode.
Is it possible to use the DCPL_XOSC pin of the CC1120 to supply the TCXO ?
If yes, I guess the TXCO voltage must be 1.8V ? do you have the tolerance associated for this supply voltage ? Or any restrictions using it ?
Best regards