Hi there,
We ran into a packet loss issue with CC1110, could you advise?
Bench setup:
1. 915 MHz in Frequency Hopping mode.
2. LPRF has 10dB transmit power.
3. A wire connects the LPRF and DUT's attennas with about 75dB attenuators in between.
4. IRQ_DONE is enabled and used to indicate a packet has received.
Observation:
1. the packet loss is about 1-2%.
2. The reason for the packet loss is due to the bad CRC, bit7 of the second byte appended after the data some time came back with 0.
Thanks,
Yi Liu