Hello ,
im confused about the term RSSI.I Suppose it is the strength of the received power at the receiver end.I did a basic experiment.i have a cc1200module connected to trxeb board.i connected the two boards antenna out through a SMA Cables.The datasheet quotes that the transmitter sends out signal at 14Dbm.But when i run the PER Test code at boards,i got a RSSI of -9Dbm even when the boards are connected through SMA cables.Im sure that the cables wont be having a loss of ''23Db''.So i connected the antenna and run the same code,i got a RSSI of -6Db,when the boards are pretty close at same orientation.(4cm away).So what is actually RSSI?And why im getting a loss of more than 23dbm when i connect through cables.Please reply..Thank you..