What would be the maximum symbol rate of the cc1310? Will it support long packets (infinite packet length mode)?
I am now using the cc1101 as a transmitter at 1Mb/s 2FSK in infinite packet length mode. I would love to migrate to the new cc1310 but that depends on the availability of a 1Mb/s data rate in 2FSK or 2GFSK and on the ability to send long packets (1024 bytes). I know that the cc1101 is only specified up to 500kb/s, but it does 1Mb/s on transmit without a problem at the maximum deviation of 380kHz.
Thanks, Sivan Toledo