This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Spurious Fail CC1200DK ARIB T108

Other Parts Discussed in Thread: CC1200DK, CC1200

Hellow.

A kit is used at present, measurement of ARIB T108.

Spurious measurement of 710MHz-900MHz doesn't enter the stipulated value and is in trouble in it.
Measurement is as a result of the fail by our development board. Next when measuring in CC1200DK, it's the same situation.

A result of measurement and register setting are as follows.

A result of measurement of CC1200DK.

11:09:56.275  RESET
11:09:56.322  FS_CAL0          0x0e 2 W
11:09:56.322  FS_CAL1          0x40 2 W
11:09:56.322  FS_CFG           0x12 2 W
11:09:56.322  FS_DIG0          0xab 2 W
11:09:56.322  FS_DIG1          0x07 2 W
11:09:56.322  FS_DIVTWO        0x03 2 W
11:09:56.322  FS_DSM0          0x33 2 W
11:09:56.322  FS_DVC0          0x17 2 W
11:09:56.322  FS_PFD           0x00 2 W
11:09:56.322  FS_PRE           0x6e 2 W
11:09:56.322  FS_REG_DIV_CML   0x1c 2 W
11:09:56.322  FS_SPARE         0xac 2 W
11:09:56.322  FS_VCO0          0xb5 2 W
11:09:56.322  IF_ADC0          0x10 2 W
11:09:56.322  IF_ADC1          0xee 2 W
11:09:56.322  XOSC1            0x03 2 W
11:09:56.322  XOSC5            0x0e 2 W
11:09:56.322  AGC_CFG0         0x84 2 W
11:09:56.322  AGC_CFG1         0x16 2 W
11:09:56.322  AGC_CFG2         0x20 2 W
11:09:56.322  AGC_CFG3         0xb1 2 W
11:09:56.322  AGC_CS_THR       0x01 2 W
11:09:56.322  AGC_GAIN_ADJUST  0x00 2 W
11:09:56.322  AGC_REF          0x2f 2 W
11:09:56.322  ASK_CFG          0x0f 2 W
11:09:56.322  CHAN_BW          0x02 2 W
11:09:56.322  DCFILT_CFG       0x26 2 W
11:09:56.337  DEVIATION_M      0x99 2 W
11:09:56.337  SYMBOL_RATE0     0x99 2 W
11:09:56.337  SYMBOL_RATE1     0x99 2 W
11:09:56.337  SYMBOL_RATE2     0xc9 2 W
11:09:56.337  FREQ0            0x5c 2 W
11:09:56.337  FREQ1            0x0f 2 W
11:09:56.337  FREQ2            0x5c 2 W
11:09:56.337  FREQOFF_CFG      0x20 2 W
11:09:56.337  IFAMP            0x0d 2 W
11:09:56.353  IF_MIX_CFG       0x18 2 W
11:09:56.353  IQIC             0x00 2 W
11:09:56.353  MDMCFG0          0x05 2 W
11:09:56.353  MDMCFG1          0x42 2 W
11:09:56.353  MDMCFG2          0x00 2 W
11:09:56.353  MDM_TEST         0x00 2 W
11:09:56.353  MODCFG_DEV_E     0x05 2 W
11:09:56.353  PA_CFG0          0x56 2 W
11:09:56.353  PA_CFG1          0x7f 2 W
11:09:56.353  PKT_CFG0         0x20 2 W
11:09:56.353  PKT_CFG1         0x03 2 W
11:09:56.353  PKT_CFG2         0x00 2 W
11:09:56.353  PKT_LEN          0xff 2 W
11:09:56.353  PREAMBLE_CFG0    0x8a 2 W
11:09:56.353  PREAMBLE_CFG1    0x20 2 W
11:09:56.353  SYNC0            0xde 2 W
11:09:56.353  SYNC1            0x51 2 W
11:09:56.353  SYNC2            0x0b 2 W
11:09:56.353  SYNC3            0x93 2 W
11:09:56.353  SYNC_CFG0        0x13 2 W
11:09:56.353  SYNC_CFG1        0xa8 2 W
11:09:56.353  TOC_CFG          0x03 2 W
11:09:56.368  setRegPacketTx
11:09:56.368  AGC_CFG3         0xb1 2 W
11:09:56.368  MDMCFG0          0x05 2 W
11:09:56.368  MDMCFG1          0x42 2 W
11:09:56.368  PKT_CFG0         0x20 2 W
11:09:56.384  PKT_CFG1         0x03 2 W
11:09:56.384  PKT_CFG2         0x00 2 W
11:09:56.400  FIFO_CFG         0x00 2 W
11:09:56.400  FS_DIG0          0x55 2 W
11:09:56.400  FS_DIG1          0x04 2 W
11:09:56.400  IOCFG2           0x06 2 W
11:09:56.400  PREAMBLE_CFG1    0x14 2 W
11:09:56.400  SERIAL_STATUS    0x00 2 W
11:09:56.400  FREQOFF_CFG      0x20 2 W
11:09:56.400  MDMCFG1          0x42 2 W
11:09:56.400  CFM_TX_DATA_IN   0x00 2 W
11:09:56.400  IOCFG0           0x3c 2 W
11:09:56.415  PA_CFG0          0x56 2 W
11:09:56.415  PA_CFG1          0x7f 2 W

11:10:02.312  FREQ0            0x0a 2 W
11:10:02.312  FREQ1            0x17 2 W
11:10:02.312  FREQ2            0x5c 2 W

11:10:06.399  SYMBOL_RATE0     0xe1 2 W
11:10:06.399  SYMBOL_RATE1     0x7a 2 W
11:10:06.399  SYMBOL_RATE2     0xa4 2 W
11:10:06.399  PA_CFG0          0x52 2 W

11:10:07.725  SYMBOL_RATE0     0xe1 2 W
11:10:07.725  SYMBOL_RATE1     0x7a 2 W
11:10:07.725  SYMBOL_RATE2     0xa4 2 W
11:10:07.725  PA_CFG0          0x52 2 W

11:10:09.581  DEVIATION_M      0x48 2 W
11:10:09.581  MODCFG_DEV_E     0x04 2 W

11:10:12.425  PA_CFG0          0x56 2 W
11:10:12.425  PA_CFG1          0x7c 2 W

11:10:14.766  SIDLE
11:10:14.766  SFTX
11:10:14.797  PKT_CFG2         0x00 2 W
11:10:14.828  AGC_CFG3         0xb1 2 W
11:10:14.828  MDMCFG0          0x05 2 W
11:10:14.828  MDMCFG1          0x42 2 W
11:10:14.828  PKT_CFG0         0x20 2 W
11:10:14.828  PKT_CFG1         0x00 2 W
11:10:14.828  PKT_CFG2         0x01 2 W
11:10:14.844  FIFO_CFG         0x00 2 W
11:10:14.844  FS_DIG0          0x55 2 W
11:10:14.844  FS_DIG1          0x04 2 W
11:10:14.844  IOCFG0           0x09 2 W
11:10:14.844  IOCFG2           0x08 2 W
11:10:14.859  MDMCFG1          0x06 2 W
11:10:14.859  FREQOFF_CFG      0x20 2 W
11:10:14.859  PREAMBLE_CFG1    0x20 2 W
11:10:14.859  CFM_TX_DATA_IN   0x00 2 W
11:10:14.859  SERIAL_STATUS    0x00 2 W
11:10:14.875  MDMCFG2          0x00 2 W
11:10:14.890  MDMCFG0          0x05 2 W
11:10:14.890  PKT_CFG0         0x20 2 W
11:10:14.890  PKT_CFG2         0x01 2 W
11:10:14.890  MDMCFG1          0x06 2 W
11:10:14.890  SERIAL_STATUS    0x08 2 W
11:10:14.890  PREAMBLE_CFG1    0x00 2 W
11:10:14.890  IOCFG2           0x08 2 W

11:10:18.159  MDMCFG0          0x05 2 W
11:10:18.159  PKT_CFG0         0x40 2 W
11:10:18.159  PKT_CFG2         0x02 2 W
11:10:18.159  MDMCFG1          0x46 2 W
11:10:18.159  SERIAL_STATUS    0x00 2 W

11:10:30.472  STX

11:10:44.591  SIDLE
11:10:44.591  SFTX

Please tell me solution method.

Best Regards,

N.Ozaki