Hi All,
In my case,my platform is DK-TM4C129X and CC1200, I have already successfully create peer-to-peer communication,then I want to complete AP-ED demo.
SMPL_Init(ReceiveCallback); // this part is the callback function Init .
static uint8_t ReceiveCallback(linkID_t sLinkID)
{
if (sLinkID)
{
g_ucPeerFrameSem++;
}
else
{
g_ucJoinSem++;
}
}// this part is the Callback function,
in IAR debug mode, when I reset the ED, the GPIOD0 INT occured, then RxISR do well , but when I set a breakpoint to g_ucJoinSem++ here, the program cannot reach here, this cause the if (g_ucJoinSem && (g_ucNumCurrentPeers < NUM_CONNECTIONS)) cannot reach, so I don't know why, why the callback function don't work, this means the callback handle has some problem?? or the smpl_config.dat has some problem?