This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200 - Observed spurious emission at 828 MHz when transmitting at 868 MHz

Other Parts Discussed in Thread: CC1200, LM317

Hi,


I designed a tiny board based on the CC1200 transceiver.

The BOM, the PCB stack-up and the PCB layout are identical to the evaluation board.

When transmitting at 868 MHz we are measuring a spurious emission at 828 MHz.

The power level of the spurious emission is -54 dBm which is very close to the EN 300 220 limit of - 55 dBm.

TRANSMISSION DATA:

Carrier frequency: 868 MHz

Output power: 14 dBm

Modulation: 2-FSK

Frequency deviation: 4 KHz

Bit rate: 1.2 kbps

Mode: High performance

TCXO: CTS 520L15IA40M0000 - Frequency 40 MHz - Frequency tolerance +/- 2 ppm

Power supply: +3.3 V - LM317

Power supply filter - LC as in the evaluation board

INSTRUMENTATION:

Spectrum analyzer: HP 8566 B - Calibrated

RBW Filter: 100 KHz - As required by EN 300 220

10 dB attenuator - Non present even though it required by EN 300 220

SPURIOUS EMISSION:

Frequency: 828 MHz

Power level: -54 dBm

EN 300 220 limit: - 55 dBm.

I'm very close to the EN 300 220 limit of - 55 dBm.

Question 1

How can I fix the problem?

Question 2

With a 3 GHz scope I noticed that the +3.3 V supply line, during transmissions, has a residual ripple of 300 mV at a frequency of 868 MHz

Is it a power supply problem?

Question 2

868 - 828 = 40 MHz

It seems it is a problem related to the TCXO which works at 40 MHz.

Am I right?

Best Regards,

Enrico Migliore

  • Hi,

    The spec limit for EN300 220 IS -54dBm (4 nW). That means still you meet the spec even with -54dBm.

    Yes, this is th ereference spur from the xtal. The spur level can be reduced further by using the following Reg settings.

    FS_DIG0=0x55

    FS_DIG1=0x04

    Plaese note that there is a trade-off in between the spur level and the phase noise by using the abovr Reg settings.

    Thanks,

    PM