It is often necessary in engineering debug and production test to turn on a steady state unmodulated carrier. Turning on CW power in the CC1200 could have been an automated operation as simple as setting a single register bit or performed via a command strobe. Texas Instruments apparently did not provide that function, and it must be achieved by a work around that involves a number of steps.
This is not described in the User Guide, but I describe below what would seem to be the necessary detailed procedure for turning on a CW carrier in the CC1200. I would appreciate it if you might look it over and comment as to whether you think it is correct. There is an open question on a possible need to redefine GPIO0 differently in order for it to be a valid input.