This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

why C1110 partnum change to C1111 ?

In my design, the C1110 runs at a main clock of 26MHz. But sometime, after power up or reset, the clock changes to 13MHz.

then all the peripherals runs base on 13MHz, including the uart0, uart1, etc.

I check all the register related to clock and osclator, they are the same at both condition.

SO, I check the PARTNUM register, I find that it was read as 0x11, but it ougth to be 0x01 for C1110.

Can anyone tell me what's wrong with the component ?