This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101 sometimes draws too much power during WoR

Other Parts Discussed in Thread: CC1101, TEST2

We use a CC1101 for 868MHz communications. While being in the wake on radio state the devices sometimes uses 1,8mA@3.2V. During that time the XOSC_stable signal on a GDO pin is low. Usually it happens for 1s (WoR interval), two or three times per hour. Sometimes the CC1101 stays in this state for minutes or hours. 

The schematics are according to the reference design 1.0.

Here the configuration during WoR:

0x00 ; IOCFG2 ; 0x2E
0x01 ; IOCFG1 ; 0x2B
0x02 ; IOCFG0 ; 0x06
0x03 ; FIFOTHR ; 0x0E
0x04 ; SYNC1 ; 0xD3
0x05 ; SYNC0 ; 0x91
0x06 ; PKTLEN ; 0xFF
0x07 ; PKTCTRL1 ; 0x80
0x08 ; PKTCTRL0 ; 0x01
0x09 ; ADDR ; 0x00
0x0A ; CHANNR ; 0x00
0x0B ; FSCTRL1 ; 0x08
0x0C ; FSCTRL0 ; 0x0A
0x0D ; FREQ2 ; 0x21
0x0E ; FREQ1 ; 0x46
0x0F ; FREQ0 ; 0xE4
0x10 ; MDMCFG4 ; 0x7B
0x11 ; MDMCFG3 ; 0x22
0x12 ; MDMCFG2 ; 0x82
0x13 ; MDMCFG1 ; 0x22
0x14 ; MDMCFG0 ; 0xF8
0x15 ; DEVIA ; 0x51
0x16 ; MCSM2 ; 0x07
0x17 ; MCSM1 ; 0x0F
0x18 ; MCSM0 ; 0x08
0x19 ; FOCCFG ; 0x16
0x1A ; BSCFG ; 0x6C
0x1B ; AGCCTRL2 ; 0x43
0x1C ; AGCCTRL1 ; 0x40
0x1D ; AGCCTRL0 ; 0xB2
0x1E ; WOREVT1 ; 0x87
0x1F ; WOREVT0 ; 0x6B
0x20 ; WORCTRL ; 0xF8
0x21 ; FREND1 ; 0xB6
0x22 ; FREND0 ; 0x10
0x23 ; FSCAL3 ; 0xEA
0x24 ; FSCAL2 ; 0x2A
0x25 ; FSCAL1 ; 0x00
0x26 ; FSCAL0 ; 0x1F
0x27 ; RCCTRL1 ; 0x41
0x28 ; RCCTRL0 ; 0x00
0x29 ; FSTEST ; 0x59
0x2A ; PTEST ; 0x7F
0x2B ; AGCTEST ; 0x3F
0x2C ; TEST2 ; 0x81
0x2D ; TEST1 ; 0x35
0x2E ; TEST0 ; 0x09

here a picture of the power consumption: