Hi everybody,
I’m working on two boards, one with a single CC1200 and another with a CC1200 and a PA, the CC1190.
My basic configuration is:
Baud rate: 9600bps
Carrier Frequency: 868MHz
Deviation: 2.4 kHz
Modulation format: 2-GFSK
RX Filter Bandwidth: 25 252Hz
I have some trouble with the advance setup of the CC1200:
- How should set the Cut-off frequency of the high pass DC filter in the DCFILT_CFG register?
- Should I limit the minimum and maximum gain on the AGC in the AGC_CFG3/2 registers?
- How could I calculate the intermediate frequency configuration in the IF_MIX_CFC register?
I know the setup will be different because I’m using a PA.
Thanks in advance
Grégory