Hello,
I have finally started on CC1310DK. To make sure that the environment is operational, running PacketSniffer R.2.18.1 and pair of CC1310EM on the SmartRF06s. I have the boards running the pre-programmed Range Test without any errors, however the Packet Sniffer does not catch any packets. I cannot find any setup information (except 868MHz) for the sniffer. In the Radio configuration->Select File window I can see only SimpliciTI files.Please advise how to set it up for the Range Test.
Thank you,
Dalibor