Howdy,
Generating a design to use the CC1120+CC1190 for sub-1GHz wireless communication and have a question about power requirements.
There are multiple reference designs and recommendations to use the TPS62730 step down converter to power the CC1120 and allow it to operate in a low power state. According to the datasheet the CC1120 has a max output power of +14dBm but we will be using an output power of +10dBm to interface with the CC1190. The datasheet specs the CC1120 at 34mA TX current @ +10dBm and a peak RX current of 22mA. The TPS62730 has a max output current of 100mA which is fine for this application.
However, to get the desired output power of +27dBm we need to use the CC1190 in conjunction with the CC1120. The CC1190 has a receive current of 3mA but a TX current of 302mA at +27dBm. This is over the spec of the TPS62730.
Questions: Can I still use the TPS62730 on the CC1120 only and power the CC1190 with a differnt 3.3V source? Or is it best to totally avoid the TPS62730 and use the same 3.3V source for both the CC1120 and CC1190. If I use the TPS62730 on only the CC1120 will this affect performance?
Regards,
Dakotah