Hello,
I'm working on W-MBUS with CC1310 (c mode). I'm able to transmit the packets, but can't receive them. I have the same code as in rfPacketRx example. I also copied my rf settings to this example code and it still can't receive any packet.
Here are my settings:
// CMD_PROP_RADIO_DIV_SETUP rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup = { .commandNo = 0x3807, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .modulation.modType = 0x1, .modulation.deviation = 0xb4, .symbolRate.preScale = 0xf, .symbolRate.rateWord = 0x10000, .rxBw = 0x24, .preamConf.nPreamBytes = 0x4, .preamConf.preamMode = 0x0, .formatConf.nSwBits = 0x20, .formatConf.bBitReversal = 0x0, .formatConf.bMsbFirst = 0x1, .formatConf.fecMode = 0x0, .formatConf.whitenMode = 0x0, .config.frontEndMode = 0x0, .config.biasMode = 0x1, .config.bNoFsPowerUp = 0x0, .txPower = 0xa73f, .pRegOverride = pOverrides_CMD_PROP_RADIO_DIV_SETUP, .centerFreq = 0x0364, .intFreq = 0x8000, .loDivider = 0x05, }; // CMD_FS rfc_CMD_FS_t RF_cmdFs = { .commandNo = 0x0803, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .frequency = 0x0364, .fractFreq = 0xf333, .synthConf.bTxMode = 0x0, .synthConf.refFreq = 0x0, .__dummy0 = 0x00, .midPrecal = 0x00, .ktPrecal = 0x00, .tdcPrecal = 0x0000, }; // CMD_PROP_RX rfc_CMD_PROP_RX_t RF_cmdPropRx = { .commandNo = 0x3802, .status = 0x0000, .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx .startTime = 0x00000000, .startTrigger.triggerType = 0x0, .startTrigger.bEnaCmd = 0x0, .startTrigger.triggerNo = 0x0, .startTrigger.pastTrig = 0x0, .condition.rule = 0x1, .condition.nSkip = 0x0, .pktConf.bFsOff = 0x0, .pktConf.bRepeatOk = 0x0, .pktConf.bRepeatNok = 0x0, .pktConf.bUseCrc = 0x0, .pktConf.bVarLen = 0x0, .pktConf.bChkAddress = 0x0, .pktConf.endType = 0x0, .pktConf.filterOp = 0x0, .rxConf.bAutoFlushIgnored = 0x1, .rxConf.bAutoFlushCrcErr = 0x0, .rxConf.bIncludeHdr = 0x0, .rxConf.bIncludeCrc = 0x0, .rxConf.bAppendRssi = 0x0, .rxConf.bAppendTimestamp = 0x0, .rxConf.bAppendStatus = 0x0, .syncWord = 0x543d54cd, .maxPktLen = 0x7d, // MAKE SURE DATA ENTRY IS LARGE ENOUGH .address0 = 0xaa, .address1 = 0xbb, .endTrigger.triggerType = 0x0, .endTrigger.bEnaCmd = 0x0, .endTrigger.triggerNo = 0x0, .endTrigger.pastTrig = 0x0, .endTime = 0x00000000, .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx };
Best regards!