This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sub 1GHz low cost Mesh Network.

Other Parts Discussed in Thread: CC1101, MSP430G2533, SIMPLICITI, TIMAC, CC2530

Hello,

I want to use CC1101 and MSP430G2533 (Given in this link:
 )
for linear mesh networking.application (i.e. like street light network automation).So, I have some question regarding this:

1) How many devices can be supported for reliable mesh network communication?

2) Is this solution useful for linear mesh communication?

3) Which communication protocol is used in this solution (like 802.15.4 or TIMAC, SimpliciTI or TI proprietary protocol)

4) Is this Sub-1Ghz Low Cost Mesh Network a complete protocol stack or just a small portion?

5) Can this stack be used on any other controller apart from MSP430G2533 or apart from MSP family?

6) MSP430G2533 has maximum 16KB of flash. Does the complete stack of Sub-1Ghz Low Cost Mesh Network solution fit in this controller? Any idea how much memory does it take?

7) What kind of data security is built in Sub-1Ghz Low Cost Mesh Network solution?

8) If I use this solution for the range of 865-867MHz for street light application, will it have any interference problems? How good is this device for interference prone environment? Is it better compared to the TI CC25xx devices in 2.4GHz range?

9) How about the range? For same output power, does it give better range compared to, say, CC2530 based solution?