This is similar to some posts, but I did not see a complete answer. I am looking at a design that uses a 1310 and a 2650. For the 2650, it might be necessary to go below the 2400 MHz that is shown in the data sheet graphs- is there any way to know what the PLL limits are?
Likewise for the 1310 it is necessary to operate from 400-433 MHz. I saw the following in another post:
The following frequency bands will be supported:
902-930 MHz
863-876 MHz
779-787 MHz
470-510 MHz
430-435 MHz
315 MHz
I understand "supported", but what is "possible"?
I also saw this in the technical reference manual:
The CC26xx and CC13xx device family provides a highly integrated low-power 2.4-GHz radio transceiver
with support for multiple modulations and packet formats. The CC13xx provides similar functionality
optimized for the sub-1 GHz bands and also allows limited operation in the 2.4-GHz band.
That would be pretty cool functionality- any idea when such a device might arrive?