This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 recommended antenna and design

Other Parts Discussed in Thread: CC1310

I'm starting to develop an embedded system based around the CC1310, but I'm not sure which antenna/antenna setup I should use. 

My aim is to develop a platform using this part that can be used in both the Americas and Europe. Ideally having one peice of hardare/one BOM to avoid manufacturing two parts and going through certification twice.

Ideally I'd like to use a small chip antenna if that was possible; saving space is important. Is there any recommended for use with the CC1310? Would one antenna work for both 868 MHz and 915 MHz bands?