When looking for crystals that meet the specifications of the cc1310 I found the Epson TSX-3224 24.0000MF20G-AC3 which has a load capacitance of 9pF. My first question is whether I should I set the config value such that CL_int = 9pF? ( my only concern is where to take into account the parasitic capacitance)
Also, I am confused why the crystal on the cc1310 launchpad (TSX-3225 24.000MF15X-AC3) has a load capacitance of 15 pF? It says in the "Configuring the CC1310 for different crystals" app note that " For reliable operation, TI recommends operating the crystal with CL from 5 to 9 pF".
Being equivalent in all cases except the CL, which crystal should i pick?