I have the CC1310 Evaluation modules, I connected a Tx unit's antenna out to Rx unit antenna using a RG316 cable with SMA connector on both ends.
I set the Tx power to -10dBm.
On the receiver the Rssi is -14
I thought the cable has an attenuation and hence increased the Tx power to -6dBm but still the Rx Rssi is -14dBm
I am using a modified version easylink example code to get the Rssi from the received packet.
CC1310 datasheet says Rx saturates at 10dBm. Does it mean that we can sense Rssi upto +10 or is it some how capped at -14dB at the code level?