This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sverre,
Thank you for you quick reply.
I am still not sure whether you meant a soft correlator (as WaveMatch) or bit based correlator?
It sounds that you meant the bit based correlator, but is there a way to detect a signal using soft correlation which achieves much better in performance?
Thanks
Just to make sure..
Does the hard sampling occur at each sample (in this case in low SNR "1" might turn into "1110") and then the detection is on 4X hard samples correlation (where X is the length of the syncword), where the incoming samples are correlated with a whole sequence of a (x4) duplicated sequence of the sync word
or
The hard decision is occurs at each bit and then the detection is based on X-length hard bit correlation
Just to summarize, there are three basic levels of sync that can be achieved:
1. Pure soft correlation with threshold - (which I understand isn't the case)
2. Hard decision upon each sample, and then 4X-length correlation with a duplicated version of the sync word bits.
3. Hard decision upon each bit, and then X-length bit-correlation.
I understand from your answer that the CC1310 uses (2) or (3), just want to make sure which one.
BTW, from what I understand, the WaveMatch in CC12x does soft-symbol correlation. Am I right, or is it more like method (2)?
Thanks again!
Dan.