This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPC for 434MHz band

Genius 3985 points
Other Parts Discussed in Thread: CC1310, CC1120, CC1200

Hi,

anybody who knows if Murata/Johan. plan for a 434 MHz IPC?

Asked 3 years agon without any hope left, perhaps meanwhile ...?

regard

GGA

  • For CC1120/ CC1200 we decided not to make one. For CC1310 the plan is make one but it's behind a couple of other things in the pipeline.
  • GGA, 

    I am also waiting for such an IPC and I'm glad to see TER's response that there is still a plan to release one. I did get two not-so-optimistic responses from Johanson about this (the picture at Murata might be different). 

    In July I got the following response from Johanson to essentially your question (434 IPC for CC1310):

    we currently have no plans to develop such a part as we do not see sufficient market demand. 

    In December 2013 I asked about an 434MHz IPC for the cc1200, and this is the response I got from Johanson back than:

    We have not released a 433 MHz version of this matched balun because we have found LTCC Networks  do not couple well at these lower bands. Although we have some passive components at these lower frequencies, they are typically much larger in size or have wider bandwidths in comparison to our L-Band + families.

    Regards, Sivan