Other Parts Discussed in Thread: CC1310, BQ25570, BQ25505, BQ25504, LAUNCHXL-CC1310, CC3100MODBOOST, CC110L, CC3200-LAUNCHXL
Hello,
I just knew about Sub 1GHz last week and got interested about its long range feature.
Since than I have many bugs in my head but I was not able to find many details about it on web...
First one is related to data protocols that I've being using in existent iot applications. My existent own devices and applications is using MQTT, CoAP, Websocket and recently LWM2M.
Suppose that I will build new Sub-1GHz devices using the CC1310 chip.
1) It would be possible to use those protocols with them ?
2) What kind of changes (devices) would be necessary to make in server machine (on local network) and application in order to receive the data from both existent devices and new sub-1ghz ones?
3) The plan is to use solar harvesting in those new devices and I will use one of BQ25505, BQ25504 or BQ25570. Since those chargers are also boost converters that works in a frequency around 1000Khz, would them cause noise/interference on CC1310 communications ?
many thanks
| BQ25505 |