Hello,
I'm attempting to use the built-in range tests for the CC1310DK I purchased to verify its range, but I can only get to about 100m out of the box before almost all packets are lost. For our eventual application we need up to 2km range. The CC1310DK advertises 20km out of box range.
The background noise I get at 1m distance with the Tx off @ 868MHz 50kbps RSSI = -100 dBm
With Tx on I get RSSI = -55 dBm.
In addition, every time I start SmartRF Studio, it tells me that my version of the board is out of date or defective and to contact TI, yet I can still use the control panel as far as I can tell.
I have read some other posts about the CC1310's range that mention defective antennae or other problems. I'm relatively new to RF as well so any help is appreciated.
Thanks