Hi all
I am using cc1310 but I am wondering that " does cc1310 have postamble when transmit data? and how many bytes postamble?"
because I read datasheet cc1310 but i can not see where postamble was writen
can you help me?
Thanks and Regards
Thanh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As far as I can see from the datasheet SPIRIT1 only sends postamble using WMBUS. CC1310 sends postamble if using the patch described here: www.ti.com/.../swra522
Dear TER,
i have a project that i use transmit and receive data from 1 CC1310 to other CC1310 by T1 mode in WMBUS mod and i configurate RF following " " www.ti.com/.../swra522a.pdf "" with 100kbps symbol rate, therefore i can transmit and receive data by T1 Wmbus.
But with that configurator and i only change symbol rate 50kbps , then i can not transmit and receive data again
Thus, i can not understand why i can transmit and receive data when i set only 100kbps but with other symbol rate that can not???
although CC1310 supports from about 2 kbps to 500 kbps running GFSK.
do you understand my problem?
i hope that you can help me
thanks and best Regards!
Thanh
if you are using the patch provided in swra552 this is only for WMBUS C and T mode which uses 100 kbps.
CC1310 can use a lot of PHYs. The phy I referred to is described in 23.7 in the TRM. The patch described in the app note is a different phy and for this only the datarates supported by that given patch can be used. Since 50 kbps is not WMBUS T or C mode this is not supported by the patch described in the app note.