Hi,
How do we check if CC1310's external 24Mhz and 32khz crystal are running properly?
Our customer's board needs to be provided to the Crystal maker for the Crystal Macthing tests
in order to find out the oscillation allowance, oscillator stability etc of the crystals on the custom board.
(in case of MSP430 devices we used to get a complete Crystal Macthing report from the crystal maker)
Is CC13XXWARE's amplitude measurement is the only way to test the crystals?
Does the below "not to measure on the 24 MHz XTAL" condition apply also to CC1310?
processors.wiki.ti.com/.../CC26xx_Tips_and_Tricks
And can we assume both 24Mhz and 32khz will start oscillation after power-up without any
register settings in the software?
Best Regards
Kummi