Hello TI employees.
Our company is developing RF transceiver using CC1310.
While using HSM of CC1310, some questions were arised.
It would be appreciated if anyone could answer the questions.
Here are the questions.
1. What's the modulation scheme of HSM?
2. Does HSM adopt channel coding? If so, then what scheme is used?
3. How much overhead(includig syncword and preamble) is included in the HSM?
4. Regarding the receiver sensitity, I have confirmed that the sensitivity level is -84dBm in this forum.
But I couldn't see the BER which resulted in -84dBm. I want to know the specification on the receiver sensitivity of HSM.
5. Does TI support the HSM in RF studio? If so, I want to know the approximate schedule of the software release.
6. I heard that the 1.6Mbps example using 4FSK scheme is possilbe in this forum.
See below link.
https://e2e.ti.com/support/wireless_connectivity/proprietary_sub_1_ghz_simpliciti/f/156/t/541825
If this is true, Can I get the example code?
I am sorry that there are a little bit many questions but please let me know the answers.
Thank you in advance.