Hi Folks,
I am currently working on developing street light system based on cc1310. I already have Zigbee based solution but I find range will be a limiting factor there and would like to have sub 1ghz solution ready there. I tend to go with TI-15.4 stack as it is straight forward, but I am worried that having no mesh capabilities will be a limiting factor? Few points to consider:
- I feel if I get 1 km radius, I am happy. I can cover most. ~150 lights is okay for me. Also very low data rates.
- The nodes can be outside mounted or soldered down on LED driver.
- IP compatibility is not an issue. Using proprietary protocol is okay for me for now.
- The nodes will be mounted a bit high on the poll so I assume less noise? This is for Indian applications to begin with.
Anything else I should consider? Would TI-15.4 be a good choice? I really need help here..
Thanks!