hi, im using MSP430F2274 in ez430-RF2500 module with code composer studio V4. i did several example programs related to msp430F2274 controller which are working perfectly...so now i am working on the wireless temperature sensor demo code. .after following the steps in readme document i successfully build the project ..but when coming to the debug part ..it is not detecting the end device and continously blinking the two leds (red and green ) and going in critical section ...in hyperterminal it is constantly displaying the access point temperature and it is unable to detect the end device and access it..
could any one please resolve my problem .....and explain the working of simpliciti network...please could any one reslove this....
thank you