This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can CC13XX MCUs be configured to use any base frequency inside 865-867 MHz band ?

Other Parts Discussed in Thread: CC1350, CC1310

1. Can CC13XX (CC1310, CC1350) MCUs be configured to use any base frequency inside 865-867 MHz band ?


2. If your answer to query number 1 is yes, then please mention, which software tool is used for configuring.


3.a. Is it possible to run any Sub-1 GHz mesh network on CC13XX MCUs ? If yes, then whic ones ?

3.b. Could you please suggest any open source Sub-1 GHz mesh network for CC13XX MCUs, in which two end nodes (placed in each other's rf range, physically) can communicate with each other without requiring any third node (be it a gateway device or an edge router etc.) ?

3.c. Could you please suggest any propreitary (or TI based) Sub-1 GHz mesh network for CC13XX MCUs, in which two end nodes (placed in each other's rf range, physically) can communicate with each other without requiring any third node (be it a gateway device or an edge router etc.) ?

Thanks in advance.