Hello, sorry I don't have xds100v3, I have JLINK V8 ,it looks support CC1310, so I just want to confirmed that my chip rev is B;
2) Removed limitation on frequency bands supported in CC1310. New frequency bands are supported for the CC1310 from die Rev B and onwards, starting with support for frequency bands in the 430-510 MHz range. This will allow customers to use the same device in a number of markets worldwide. Note that current die Rev A material will still be limited to 863-930 MHz only. SmartRF Studio 2.4.3 or later will detect die Rev A devices and issue an appropriate warning as to the applicable frequency range. Please remember to update SmartRF Studio accordingly.
FCFG1. ICEPICK_DEVICE_ID Register:
value is 0x2B9BE02F,and 0x242b9BE02F , so the die REV is A or B.
With my tested ,It looks them can't work at 433.92MHz, ... change to 868MHz, that is OK.