This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: RX spurious at 5.2 GHz

Part Number: CC1101
Other Parts Discussed in Thread: CC1100,

Hello,

we have an old design using the CC1100. During recertification according to EN 300 220 V 2.4.1 we saw a spurious at 5.2 GHz in RX mode with a level of -37 dBm(!), the limit is at -47 dBm.

My first attempt to reduce the level was to modify the matching. I ended with completely removing it, but the spurious level was still the same, what means that it is not radiated by the antenna. I then replaced the CC1100 by an CC1101, resulting in a little improvement, but not enough to pass EN 300 220.

I also measured the SmartRF04EB with different releases of the CC110XEM board and I was surprised to see the same spurious with them. That means to me that the influence of the PCB layout has no big influence on this spurious and now I don't know what else I can try to pass the test.

Does anyone have any experience with this spurious?

RX Frequency is 868.3 MHz.

  • In Rx, the 5.2 GHz spur you see is the VCO frequency leaking out. The VCO leakage is typically through VDD pins which make following the reference design regarding de-coupling caps. We have tested the CC1101 and the pass the Rx spurious limit with good margin so I'm surprised that you see a value above the limit.

    - If you provide us with schematic + layout we can review and come with recommendations on what can be done. If you don't to post directly on the forum, send me a friend request.
    - Could you post the results you got on your board and on the EM?
  • Current return path.pptWhat you need to look at is the grounding strategy. Is there a solid (unbroken) ground plane going from the decoupling capacitor ground pad and back to the chip? Refer to the last slide in the attached presentation