This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 TI 15.4 stack power consumption test on sensor device

Part Number: CC1310


Hi Team, 

I'm test the power consumption on CC1310 Launchpad when running TI 15.4 stack sensor device.

My sensor device send data every 50s, after data send out it will start the polling for 5s with 1s interval. After 5s, it set the poll rate to 0.

So in the 45s duration, there was no packet sent out from sensor device, but I from my test the current is about ~30uA. It's really much high for a sensor device. 

I enable the POWER_MEAS pre-define symbols.

For the hardware setup shown as below, I removed all the jumper on the CC1310 Launchpad.

Please check the attached sniffer logs.

Thanks.

Victor Xu

Best Regards

power consumption test.zip