This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: Reducing 40 MHz clock oscillator spur levels

Part Number: CC1200


Is there a way to affect 40 MHz clock oscillator spur levels in output by tweaking some internal frequency synthesizer setting? I use external 1W power amplifier and spur levels at +-40 MHz offset from carrier are -70 dBc which is good level, but I would need to reduce them further at least by few dB to get some margin for type approval specification.