Hello,
I have some problems while studying simplelink-cc13xx-sdk.
1. How can i set data rate as another value?
2. How can i transmit broadcast message from coordinator to all sensors?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have some problems while studying simplelink-cc13xx-sdk.
1. How can i set data rate as another value?
2. How can i transmit broadcast message from coordinator to all sensors?
Best regards.
Hello Gonsalez,
If this question is not related to TI 15.4g stack, then answer is Yes, a wide range of data rates are supported. You can use SmartRF studio to test any data rate upto 500ksps. Higher data rates are also possible using specific patches.
If this question is about TI 15.4g stack
1. With the current release only 50Kbps is officially supported. There is development underway to support 5kbps in LRM (Long Range Mode). This should be available in the next release.
2. Broadcast of messages is not supported in the current release. There is a ticket in place to add this support. A future release will have support for broadcasting.
Regards,
Prashanth