Team,
A customer is planning to use CC1111 but they need -40 to +85°C temperature range support. According to this thread, it should be possible to treat CC1111 as CC1110 if USB is not used. However, they need the USB at room temperature to do the commissioning/first time configuration. Will this work?
Which crystal frequency they need to use? still 48 MHz as standard for CC1111? or 26/27? I guess 48 MHz is needed for clocking the USB interface.
Thanks.