Hello!
I'am planning to use CC1310 for the new device.
I have a similar question around CC1310 Sub-1 GHz Ultra-Low Power Wireless Microcontroller.
1) Is it possible to use one of the internal Timers for external frequency counting? Freq = 50...600Hz
Will Timer work in Shutdown mode? And if NO, Why? I'm clocking Timer from external freq.
Which of GPIO pins i will use as Timer CountPin?
2) Is it possible to use internal RTC to wake up CPU from Standby every 250mS for 2-3mS Active mode
3) In CC1310 datasheet I found following:
The Brown Out Detector is disabled between recharge periods in STANDBY. Lowering the supply voltage below the BOD threshold
between two recharge periods while in STANDBY may cause the BOD to lock the device upon wakeup until a Reset/POR releases it.
Is the WDT timer will solve this problem or it will Hang too untill RESET?
What is WDT power consuption?
Thanks a lot.
Alex