Other Parts Discussed in Thread: CC1190
Hello,
I'm making a design with the CC1310 and I'm not sure of the RF front end stage. I hesitate between all-inclusive balun solution or full discrete solution.
The SWRA524A doc shows the results of the balun use : it seems that there is a sensitivity reduction of ~2-3dB (-108dBm @ 50kbps) compared to the device specs (-110dBm).
Do you confirm the characterisation published in datasheet has been performed using the discrete front end solution implemented in the ref design ?
I've downloaded the ref design guides, but I'm not sure I can make my boards with the same stackup. In your ref design you have 0.175mm width between layer 1 and 2 or 3 and 4. In my case I can have 0.39mm (that's already the stackup I use for other boards).
May that difference force me to change the values of the discrete element network ? Should I use a coefficient to determine the width of the inter-components tracks (I'm not speaking of the final 50 Ohms track to antenna) or is it negligible ?
What about single ended design ? I did not see any example. What may be the improvements from it ?
I just need my board to be compliant with both 868MHz and 915MHz bands.
Aurelien